AnsweredAssumed Answered

TJA1043T在不同供电电压下,其工作模式疑问?

Question asked by 志明 肖 on Sep 8, 2019
Latest reply on Sep 15, 2019 by G.w. Sun

条件1:TJA1043Vbat脚设定9V,VCC和Vio脚为5V供电

STB_N和EN脚都是高电平,err_N脚为低,1043无报文;

条件2:Vbat脚电压以0.1逐渐提高,VCC和Vio脚保持5V供电

待Vbat脚电压升至10.1V时,err_N脚输出电平为高,1043有报文;

条件3:Vbat脚电压设定13V时,VCC和Vio脚为5V供电

CAN有报文;

条件4:Vbat脚电压以0.1V逐渐下降,但VCC和Vio脚保持5V供电

待Vbat脚电压降至6V时,1043才停止报文发送。

疑问:

1、芯片datasheet规定工作电压4.5~45V,为什么供电电压要在10.1V以上才会发报文出来?电压往下降却可以在6V以下才停发报文?

下图为电路设计架构图。

 

联系方式:xiaozhiming@hozonauto.com

Outcomes