我有一个编译好的elf文件,需要将它下载到MPC5748G Demo开发板里。请问S32DS 能否支持 在不建立工程的情况下,将elf文件下载到目标板?或者有没有其他下载方式。(硬件有:目标板,PE)
Hellow Alice_Wang:
The configuration of debugger is default.
Whether software Registraction has some problems?
Thanks.
Hi Miles
You have concrete board connection issue with S32DS
I suggest you ask the question in English to MPC5xxx
There are many experienced MPC5xxx engineers overseas monitor that space.
Have a nice day,
Jun Zhang
Hello Miles M ,
You can use the "Flash from file ..." button as below:
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
I tried this way. but it report error "Disconnected from......" as follows.
I also new a "hellow" projtct from example,but the reult as follows:
Hello Miles,
Does it can work well when debug a project?
Show the debugger configuration view:
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hellow Alice_Wang: