Hi,
I have a Mimxrt1050 evk development card. Can I find out which camera sensors are compatible with the card?
Does it work with the following camera sensor?
Regards
Hasan
Hello Hasan,
Can I find out which camera sensors are compatible with the card?
The i.MX RT1050-EVKB board has a 24pin connector where the camera cable needs to fit in. To know if your camera is compatible, the cable should be of 24 pins and the signals must match to the ones on the evaluation board.
Does it work with the following camera sensor?
As mentioned before, you need to have a 24-pin camera and the signals must match to the ones on the 24-pin connector of the evaluation board. For more information, I recommend you check the following page.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------