AnsweredAssumed Answered

i.mx6q ADV7180, no pobing. no/dev/video/0

Question asked by Purvi Billore on Aug 31, 2019
Latest reply on Sep 1, 2019 by igorpadykov
  1. Problem statement: The ADV7180 is interfaced with i.MX6q processor on CSI0 bus as shown in following schematic circuit. The linux version 3.14 is used (YOCTO build). The decoder adv7180 is not getting probed at kernel level and not getting attached to ipu/csi. Using UBOOT I2C, device ID 0X21 (i2c address of adv7180) is successfully probed. So there is no video device detected in /dev/video0.
  2. Schematic
  3. Processor interface

 

Decoder circuit

 

 

DTSI file: The adv7180 is connected to i2c2 port. The driver definition and pin configuration is given below,

v4l2_cap_0 {

        compatible = "fsl,imx6q-v4l2-capture";

        ipu_id = <0>;

        csi_id = <0>;

        mclk_source = <0>;

        status = "okay";

    };

 

&i2c2 {

                clock-frequency = <100000>;

                pinctrl-names = "default";

                pinctrl-0 = <&pinctrl_i2c2>;

                status = "okay";

 

                rtc@68 {

                compatible = "st,m41t00";

                reg = <0x68>;

        };

                adv7180: adv7180@21 {

                compatible = "adv,adv7180";

                reg = <0x21>;

                pinctrl-names = "default";

                pinctrl-0 = <&pinctrl_ipu1_2>;

                clocks = <&clks IMX6QDL_CLK_CKO>;

                clock-names = "csi_mclk";

                DOVDD-supply = <&vgen3_reg>; /* 3.3v, enabled via 2.8 VGEN6 */

                AVDD-supply = <&vgen3_reg>;  /* 1.8v */

                DVDD-supply = <&vgen3_reg>;  /* 1.8v */

                PVDD-supply = <&vgen3_reg>;  /* 1.8v */

                pwn-gpios = <&gpio1 17 0>;   /* active high: SD1_DAT1 */

                ipu_id = <0>;

                csi_id = <0>;

                mclk = <24000000>;

                mclk_source = <0>;

                cvbs = <1>;

                };

 

pinctrl_ipu1_2: ipu1grp-2 {

                                                fsl,pins = <

                                                               

 

MX6QDL_PAD_CSI0_VSYNC__IPU1_CSI0_VSYNC                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_MCLK__IPU1_CSI0_HSYNC                               0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_PIXCLK__IPU1_CSI0_PIXCLK            0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DATA_EN__IPU1_CSI0_DATA_EN 0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT4__IPU1_CSI0_DATA04                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT5__IPU1_CSI0_DATA05                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT6__IPU1_CSI0_DATA06                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT7__IPU1_CSI0_DATA07                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT8__IPU1_CSI0_DATA08                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT9__IPU1_CSI0_DATA09                             0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT10__IPU1_CSI0_DATA10                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT11__IPU1_CSI0_DATA11                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT12__IPU1_CSI0_DATA12                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT13__IPU1_CSI0_DATA13                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT14__IPU1_CSI0_DATA14                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT15__IPU1_CSI0_DATA15                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT16__IPU1_CSI0_DATA16                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT17__IPU1_CSI0_DATA17                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT18__IPU1_CSI0_DATA18                           0x80000000    /*custom add*/

MX6QDL_PAD_CSI0_DAT19__IPU1_CSI0_DATA19                           0x80000000    /*custom add*/

                                                >;

                                };

 

  1. Deconfig used
  2. CONFIG_MEDIA_SUPPORT=y
    CONFIG_MEDIA_CAMERA_SUPPORT=y
    CONFIG_MEDIA_RADIO_SUPPORT=y
    CONFIG_MEDIA_RC_SUPPORT=y
    CONFIG_RC_DEVICES=y
    CONFIG_IR_GPIO_CIR=y
    CONFIG_MEDIA_USB_SUPPORT=y
    CONFIG_USB_VIDEO_CLASS=m
    CONFIG_V4L_PLATFORM_DRIVERS=y
    CONFIG_VIDEO_MXC_OUTPUT=y
    CONFIG_VIDEO_MXC_CAPTURE=m
    CONFIG_MXC_CAMERA_OV5640=m
    CONFIG_MXC_CAMERA_OV5642=m
    CONFIG_MXC_CAMERA_OV5640_MIPI=m
    CONFIG_MXC_TVIN_ADV7180=m
    CONFIG_MXC_IPU_DEVICE_QUEUE_SDC=m
    CONFIG_VIDEO_MXC_IPU_OUTPUT=y
    CONFIG_VIDEO_MXC_PXP_V4L2=y
    CONFIG_VIDEO_MXC_CSI_CAMERA=m
    CONFIG_MXC_VADC=m
    CONFIG_MXC_MIPI_CSI=m
    CONFIG_MXC_CAMERA_OV5647_MIPI=m
    CONFIG_SOC_CAMERA=y
    CONFIG_VIDEO_MX3=y
    CONFIG_V4L_MEM2MEM_DRIVERS=y
    CONFIG_VIDEO_CODA=y
    CONFIG_RADIO_SI476X=y
    CONFIG_SOC_CAMERA_OV2640=y

 

Need to know valid deconfig menu to enable the video decoder driver in the kernel level. So that ADV7180 get probed and attached to the ipu/CSI and  the etc/dev/ will list Video0 for video input

Outcomes