AnsweredAssumed Answered

Using MFG Tool on Linux to flash iMX6ULL EVK

Question asked by Meetali Patel on Sep 2, 2019
Latest reply on Sep 3, 2019 by CarlosCasillas

Hello,

 

I am trying to flash a binary on iMX6ULL EVK Board using MFG Tool. When running mfgtools on Windows, there is no issue and I am able to flash successfully. However, when I trying running mfgtools on Linux, I am unable to do so (I am using Ubuntu 14.04). 

 

To run the mfgtoolcli application I executed the following command:

   $ ./mfgtoolcli -l eMMC -s lite=l -s 6uluboot=14x14evk -s 6uldtb=14x14-evk

 

The output is:

Your Options:
lite: l
6uluboot: 14x14evk
6uldtb: 14x14-evk
Ready to flash.
init op Failed code# 24

 

The logs in MfgToolLibLog.txt file are:

Start new logging
ModuleID[2] LevelID[1]: Error: Invalid device name: MX6ULL
ModuleID[2] LevelID[1]: Parse ucl script failed, error code: 24

 

Please guide me on how can I successfully flash using the mfgtools on Linux machine.

 

Thanks

Meetali Patel

Outcomes