IMX8 MINI 不能开机 无打印 IMX8 MINI cannot boot without printing

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX8 MINI 不能开机 无打印 IMX8 MINI cannot boot without printing

458 Views
刘生刘
Contributor I

The program can be downloaded successfully, but set to EMMC when it starts.

Unable to start and print, it is no problem to test DDR verification with DDR testing tools.

When burning with uuu, the program has also been burned into emmc, and the voltage of start-up configuration pin is all over normal.

Reset and crystal oscillation are also normal. What may be the cause of this situation? Is there any way to investigate it? Thank you.

Attached is the log at download time

0 Kudos
1 Reply

370 Views
kunalkotecha1
Senior Contributor II

Hi 刘生刘 ,

It seems you want to burn the images to eMMC and boot from it. Please use demo images with L4.14.98_2.0.0, as these are working in i.MX8M Mini EVK.

Let us if you still face any issue.

Regards,

Kunal

0 Kudos