AnsweredAssumed Answered

T2080 USB control signals

Question asked by Paula García-Moreno on Aug 27, 2019
Latest reply on Aug 27, 2019 by ufedor

If I don't use the USB power fault and usb power enable signals, would I have any problem with this interface?

I don't want to use them since I am using the same 5V regulator to supply USB and other devices, so I don't want USB controller to controls also those other devices.

Should I use a specific 5V source to USB so I can control it with the above mentioned signals or it is not necessary?

 

Thanks in advance.

Outcomes