For the LPC54114 audio and voice recognition kit is it possible to use the line-in audio port instead of the mic to send the Sensory keyword and commands? If so, how do I enable this?
Hi David
NXP supports questions related to the MCU hardware and drivers (DMIC interface and Hardware VAD etc.) via the internal LPC community forum. Questions about voice triggering performance and integration that is not related to the MCU hardware should be referred to Sensory.
For more, see https://community.nxp.com/docs/DOC-332211
Have a nice day,
Jun Zhang
OK, thank you for the quick response on this.
David Hille | Owner / CEO
Moderno Technologies, Inc.
(360) 624-5538
ModernoTechnologies.com
You are welcome!
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------