Communicating between 2 NHS3100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Communicating between 2 NHS3100

401 Views
michael_sprauve
Contributor I

Hi,

I was wondering if I could use the NFC module to communicate between 2 NHS3100 chips. I would like to have my two devices communicate which each other when they are brought in close proximity.

Tags (2)
0 Kudos
1 Reply

333 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hi Michael,

The NHS3100 is a passive element. This means that the NFC qualities it has is essentially a tag. Unfortunately you will not be able to communicate between two of these. You need an active element in order to properly communicate with the NHS3100. 

If you can provide the minimum requirements of your application, such as other peripherals, power, security, etc. I can point you in the right direction so you can compliment the NHS3100 correctly.

Or if you have any other questions regarding the NHS3100, do let me know as well.

Best Regards,

Sabina

0 Kudos