BT5.0 transceiver to transmit and receive the voice and music signal

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

BT5.0 transceiver to transmit and receive the voice and music signal

489 Views
mam
Contributor I

Hi,

I am looking for a BT5.0 transceiver which can help to transmit and receive the voice and music.

I already have a host IC with codec, but, just need a BT5.0 transceiver to transmit and receive the voice and music signal from the other device.

So, can KW35 or QN908x fulfill my requirement?

Arm® Cortex®-M0+|Kinetis® KW35Z/36Z Bluetooth Low Energy 32-bit MCUs | NXP 

QN908x: Ultra-Low-Power Bluetooth Low Energy System on Chip (SoC) Solution | NXP 

BR

Matthew

Labels (2)
Tags (2)
0 Kudos
1 Reply

419 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

The Bluetooth LE does not have a profile for audio, nonetheless, you might be able to use the GFSK and create your own frame like the Bluetooth LE  and adapt it to send audio through the radio as it has a 2M PHY in the QN9080 case.

Still, if you are looking for an audio solution, have you checked this device ?

Regards,
Estephania

0 Kudos