i.MX 8QuadXPlus MEK board how to use mic ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX 8QuadXPlus MEK board how to use mic ?

735 Views
wcle
Contributor I

My board is i.MX 8QuadXPlus MEK . My os is Android P9.0.0_1.0.2_AUTO_Beta.

My question is :

1.

when i use wm8960 ,

mek_8q:/system/bin # tinymix -D 0 "ALC Function" 3

mek_8q:/system/bin # tinymix -D 0 "ADC PCM Capture Volume" 230

mek_8q:/system/bin # tinymix -D 0 "Capture Volume" 60

mek_8q:/system/bin # tinymix -D 0 "Capture Switch" 1

mek_8q:/system/bin # tinymix -D 0 "Left Input Mixer Boost Switch" 1

mek_8q:/system/bin # tinymix -D 0 "Right Input Mixer Boost Switch" 1

mek_8q:/system/bin # tinycap aa.wav

Capturing sample: 2 ch, 44100 hz, 16 bit

^CCaptured 537624 frames

mek_8q:/system/bin # tinyplay aa.wav

Playing sample: 2 ch, 44100 hz, 16 bit

 

I grabbed my voice with the MIC of my headset by “tinycat aa.wav”,then tinyplay aa.wav.

i can hear it but volume is very low,why?

2.

when i use cs42888,

It's normal to play music from AUDIO OUT-FR media. You can hear the sound played by media. When using the recorder software to record,But MIC can't record the sound. 

why?

0 Kudos
1 Reply

636 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi wang,

I’m afraid that i.MX8QXP family is still on preproduction and no additional information/support could be provided yet. For further assistance, please contact with your Sales/FAE.

Additionally, Android Auto is supported under Professional Services scheme. You could refer to the following link for additional details:

NXP Professional Services | NXP 

Hope this will be useful for you.
Best regards!
/Carlos
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

-------------------------------------------------------------------------------

0 Kudos