AnsweredAssumed Answered

Yocto DISTRO Configuration for imx8mmevk

Question asked by Vijay Kumar on Aug 21, 2019
Latest reply on Aug 23, 2019 by Joan Xie

Hi,

 

I am trying to generate core-image-base for imx8mmevk board. What is the yocto DISTRO configuration needs to be used imx8mmevk board ? 

The  below part in the Yocto Project Users guide is confusing. Is it referring to i.MX8 only or i.MX8M also ?

• fsl-imx-x11 - X11 graphics are not supported on i.MX 8.
• fsl-imx-wayland - Wayland weston graphics.
• fsl-imx-xwayland - Wayland graphics and X11. X11 applications using EGL are not supported.
• fsl-imx-fb - Frame Buffer graphics - no X11 or Wayland. Frame Buffer is not supported on i.MX 8.

 

Thanks for your help in advance,

 

Regards,

Vijay.

Outcomes