i.MX8M XTALI/O internal impedance

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX8M XTALI/O internal impedance

Jump to solution
703 Views
m_c
Senior Contributor I

In the i.MX8M reference design, the resistance (R411 and R412) of XTALI/O 25M and 27M are DNP. Is that mean there has an internal impdeance in between?

pastedImage_1.png

Labels (1)
0 Kudos
1 Solution
608 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, i.MX8M has internal biased amplifier. But since value of the internal bias resistor is not 

guaranteed exactly, the reference design provides external option.

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

View solution in original post

0 Kudos
1 Reply
609 Views
Yuri
NXP Employee
NXP Employee

Hello,

Yes, i.MX8M has internal biased amplifier. But since value of the internal bias resistor is not 

guaranteed exactly, the reference design provides external option.

 

Have a great day,

Yuri

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos