AnsweredAssumed Answered

s12zvml PMSM Sensorless Report Error

Question asked by YG Y on Aug 21, 2019
Latest reply on Aug 23, 2019 by Diana Batrlova

Hello Everone!

   there is a problem relate to PMSM Sensorless ,when I use BDM DEBUG the motor program,The following error occurred, the error "xiaofan gu" Also mentioned,But I do according to file have no effect!

and the detail information is:

   

I just add a LIN module into a project,and the LIN module is "FSL_LIN_2.x_STACK",but when i didnt do this,the project work well and can debug. but when i add the LIN module into the project, the problem occured.

I check it and find when i delete this "lin_isr.c" file,COMPLIE AND Debug OK,But LIN do not normal working!

 

So,what should i do?

Any help will be appreciated!

  thanks!

Outcomes