AnsweredAssumed Answered

Voltage Level of USB1_ID and USB2_ID of i.MX 8M Mini

Question asked by Peter Lischer on Aug 19, 2019
Latest reply on Aug 19, 2019 by Yuri Muhin
Branched to a new discussion

What are the voltage levels of the dedicated USB1_ID and USB2_ID pins of the i.MX 8M Mini? I was not able to find any electrical information about these pins in the datasheet or the hardware design guide. Are these pins 1.8V logic level or 3.3V? Is there any internal pull-up or pull-down resistor?

Outcomes