AnsweredAssumed Answered

JN 5169 Tables was cleared

Question asked by wei ss on Aug 16, 2019
Latest reply on Aug 20, 2019 by wei ss

There are 30 router in the network, and has work fine 2days,and then an device(A)'s MAC was cleared from Address Map Table,Route Table and Neighbour Table.So when A report his attribute to coordinator, we can not determine who is reporting(The Corresponding Relation between MAC addr and Short Addresses on Coordinator was missed)

 

1.My envirorment:

1) SDK:JN-SW-4170 v1840
2)Coordinator:Base on JN-AN-1216-Zigbee-3-0-IoT-ControlBridge-v1011, we modify code about Uart1,RF signal handle,table size, etc.

3)30 Routers joined the network

 

 

2.Uart print some suspicious information: network status 12(sNwkStatusIndicationEvent.u8Status), no other Error logs.

 

3.The field ‘auth’(uAncAttrs.bfBitfields.u1Authenticated)change to 0

 

4.Sniffer log attach below.

Outcomes