Hi,
Is there any memory bandwidth test data for imx8mm_evk lpddr4 and ddr4?
I tested imx8mm_evk with the command bw_mem 1000M rd , the result is only 2500M / s,
bw_mem 1000M wr only 1500M / s.
The theoretical bandwidth of lpddr4 3000MT/s 32bit should be 6000M/s+. Why is imx8mm_evk only 2500M/s?
Hi li
for DDR performance one can try the following command :
perf stat -e ddr0/read-cycles/,ddr0/write-cycles/ -a
Theoretical bandwidthcan be achieved only in theory, in real life
bandwidth is restricted by processor internal buses bandwidth,
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------