AnsweredAssumed Answered

RT1064 ok instead of RT1060?

Question asked by Nick Guzzardo on Aug 15, 2019
Latest reply on Aug 22, 2019 by Juan Carlos Pacheco

I already have a few RT1064 EVKs.  Since the only significant difference that I am aware of is the 4MB of on-chip flash for the RT1064, can I use the RT1064 instead of buying the RT1060 EVK?

 

Update: I verified that eIQ is listed for the currently available RT1064 SDK, but it references a requirement for the RT1050 or RT1060 which apparently prevents it from being selected for inclusion with the SDK.  So a follow-up question:  Is it possible to use the RT1060 SDK with the RT1064 EVK?

Outcomes