Issue about the FIFO of DSPI on MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Issue about the FIFO of DSPI on MPC5744P

549 Views
qm1013
Contributor III

Hello, I have some questions about the FIFO of DSPI.

When I enable the transmit FIFO . Then write the SPI_PUSHR register with the EOQ set to 0 and the transmit FIFO is not full . Will the DSPI start sent the data immediately ? Maybe , it will start send the data when the transmit FIFO is full or the EOQ bit is set.

Am I  right?

Regards,

Meng

Labels (1)
0 Kudos
1 Reply

457 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

yes, frame is started immediately, unless any of following conditions exist:

• SR[EOQF] bit is set

• Chip is in the Debug mode and the MCR[FRZ] bit is set
• MCR[HALT] bit is set

BR, Petr

0 Kudos