eMMC lifetime with iMX6

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

eMMC lifetime with iMX6

1,108 Views
gmmo
Contributor I

This is really a memory question, but since I am using an iMX6 maybe someone can help or have used similar setup

I have an embedded system using iMX6 that uses this eMMC (8 GB) as memory for the Android BSP and application

https://media.digikey.com/pdf/Data%20Sheets/Panasonic%20Semiconductors%20ICs%20PDFs/MC_Series_NPI.pd... 

It says on the sheet:

"By Reducing The User Area Of NAND, The Total Number Of Program / Erase Cycles Increases 10x. Typical MLC NAND Is Capable Of 2K Program Erase Cycles. pSLC NAND Is Capable Of 20K."

What does it mean exactly? If the Android BSP is writing logs to it constantly (what we have) will it wear out the memory after 20K writes? This seems very little.

If anyone can give me pointers since I am trying to calculate the lifetime of our product based on this information.

thank you,

Labels (1)
Tags (1)
0 Kudos
1 Reply

847 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The lifetime you can see the emmc datasheet, from your above information, the emmc you are using can  Program / Erase 20K. If you need more you can see other emmc.

0 Kudos