AnsweredAssumed Answered

sgtl5000播放声音时i2s datain没有波形

Question asked by yun li on Aug 13, 2019
Latest reply on Aug 14, 2019 by Wigros Sun

Hi,在开发sgtl5000的过程中,linux上检测到了声卡,并用aplay ruguo32k.wav命令播放了文件,但是遇到如下的问题:

1.播放声音32000hz,16bit,算出来的i2s sclk应该是2*32000*16 = 1024000,但是量到的频率是3M多

2.i2s sclk有信号,但是播放声音时,i2s datain没波形,请看一下寄存器配置是否正确,谢谢!

sgtl5000的寄存器如下:

0xa0 0x11 0x00 0x71 0x00 0x01 0x01 0x30 0x01 0x10 0x00 0x10 0x00 0x00 0x02 0x00 0x3c 0x3c 0x3c 0x3c 0x01 0x5f 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x18 0x18 0x00 0x22 0x00 0x08 0x00 0x41 0x00 0x00 0x03 0x04 0x0f 0x0f 0x7a 0xfb 0x50 0x00 0x08 0x00 0x00 0x17 0x01 0xc0 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00 0x00

Outcomes