How can I implement S32k144 lpspi0 communication its own lpspi1 for test lpspi function is OK,is there one demo for reference,thank you.
follow is the S32 DS IDE example : lpspi_transfer_s32k144
LPSPI_DRV_MasterInit(SEND, &masterState, &Send_MasterConfig0);
LPSPI_DRV_SlaveInit(RECEIVE, &slaveState, &Receive_SlaveConfig0);
ADC_DRV_ConfigConverter(INST_ADCONV1, &adConv1_ConvConfig0);
FTM_DRV_Init(INST_FLEXTIMER_PWM1, &flexTimer_pwm1_InitConfig, &ftmStateStruct);
FTM_DRV_InitPwm(INST_FLEXTIMER_PWM1, &flexTimer_pwm1_PwmConfig);
while(1)
{
ADC_DRV_ConfigChan(INST_ADCONV1, 0U, &adConv1_ChnConfig0);
ADC_DRV_WaitConvDone(INST_ADCONV1);
ADC_DRV_GetChanResult(INST_ADCONV1, 0U, &adcRead);
slaveDataSend = (uint8_t)adcRead;
LPSPI_DRV_SlaveTransfer(RECEIVE, &slaveDataSend, &slaveDataReceive, BUFFER_SIZE);
LPSPI_DRV_MasterTransferBlocking(SEND, &masterDataSend, &masterDataReceive, BUFFER_SIZE, TIMEOUT);
FTM_DRV_UpdatePwmChannel(INST_FLEXTIMER_PWM1, 0U, FTM_PWM_UPDATE_IN_DUTY_CYCLE, masterDataReceive<<8, 0U, true);
}
Hello shen jun,
I have difficulties to understand.
Could you please elaborate?
If you want to have more information about the lpspi_transfer_s32k144 example, please refer to its documentation in the SDK installation folder:
…\S32DS_ARM_v2018.R1\S32DS\S32SDK_S32K1xx_RTM_3.0.0\doc\Start_here.html
Thanks,
BR, Daniel