TPMS_BtLdr_1 -RealTerm Dispaly"ERR=05"

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

TPMS_BtLdr_1 -RealTerm Dispaly"ERR=05"

667 Views
wentaohu
Contributor I
recently,i am working on TPMS_BtLdr_1 project ,I used FXTH87 module evaluation boards which NXP provide.
      When I debug the project "TPMS_BtLdr_1",the window come out "No source available for "0xE92F (0xE92F)() " " , and then debuger lose the connection to the FXTH87 module evaluation boards.
      The screenshot as below:
   In addition,i use RealTerm send the comand to FXTH board ,it always come out "ERR=05“,and LF wave Display normal,i guess something wrong about FXTH side,can you help me ?
   thank you !
Labels (1)
Tags (1)
0 Kudos
2 Replies

580 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Wentao,

Could you please try to attach the screenshots once again? I cannot open them.

Thank you.

Best regards,

Tomas

0 Kudos

580 Views
wentaohu
Contributor I

Hi Tomas!

   Thank you for your help!

    This problem has Solved !

    Because i used the Lib"fxth870000.c" before,when i changed the Lib "fxth870000_lib",It's works OK!

    pastedImage_1.png

Thank you all the same!

Wentao Hu.

0 Kudos