I can't seem to find any documentation/code that shows to use any of the 8-bit pulse accumulators to generate an interrupt after X number of pulses have been recieved.
I see ICPAR is used to enable 8-bit pulse accumulators, but I dont see anything on how to set interrupts after X number of edges have passed. Are there no such controlls? Does it just generate an interrupt after it overflows(255) meaning I have to avance the count in software to get it to interrupt after a specifeid number of edges have passed.
Any input would be grately appreicated.