正在学习ISO15693,购买了CLEV6630AM的开发套件,NFC Cockpit 4.8.0 盘点卡和读指定块数据都可以,但是不知道如何写数据到卡里,有一个Send Data的按钮,但不知道数据格式是怎么样的,请大家指点,谢谢!#NFC 6630A #NFC Cockpit
The problem has already been solved, thanks.
请问你是如何解决的,我现在是写数据到比如0x03块,都回来并没有改变。
而且我读任意两个块,数据都是一样的。啥问题呢?
Hello,
According to the translation of this thread, I understand that you would like to know the command needed to write data to the card. The commands are according to ISO 15693, e.g. if you would like to write one single block, the corresponding command will be 0x21 followed by the block to be written and the block data.
Hope this helps.
BR,
Ivan.
非常感谢您的回复,我尝试了在Tx data without flag输入框输入0x21 20 11 11 11 11,但是提示数据错误,详细请见图片
Hello,
Our support is worldwide, could you please translate it to English for a better understanding?
Thank you,
Ivan.