About the GPIO_EPDC_D4 (QSPIA_DQS) signal in the circuit diagram (sch-28590_i.mx7d_saber_rev_d)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About the GPIO_EPDC_D4 (QSPIA_DQS) signal in the circuit diagram (sch-28590_i.mx7d_saber_rev_d)

467 Views
goto11
Contributor III

Hello,community

Only TP10 is connected, but what is this signal used for?

Best Regards,
Goto

Labels (1)
0 Kudos
1 Reply

401 Views
igorpadykov
NXP Employee
NXP Employee

Hi GoTo

it may be used for evaluation of QSPI DQS functionality

described in sect.10.2.10 Serial Flash Data Input Timing

i.MX 7Dual Applications Processor Reference Manual

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos