AnsweredAssumed Answered

Can i move High-current source pin to any other pin?

Question asked by jtro 9 on Aug 9, 2019
Latest reply on Aug 11, 2019 by xiangjun.rong

Can i move high current source pin to other pin?

 

In User manual UM11029 Page 130

"The switch matrix also enables the output driver for digital functions that are outputs. The
electrical pin characteristics for both inputs and outputs (internal pull-up/down resistors,
inverter, digital filter, open-drain mode) are configured by the IOCON block for each pin."

 

As per above statement I assume that if i move any pin to other pin then characteristics of will remain same for that port.

for example, If i move PIO0_12 Pin - 4 (which is a high current source pin) to Pin - 11 (default is PIO1_0) then at Pin - 11 I'll able to source 20mA current. Am i right?

 

Can you please clear my doubt.

Outcomes