Customer : Larslabs (Germany)
Platform: i.MX 8M-Mini + PF8121
Hi Jinyu, one of my customers got a few unprogrammed PF8121 samples (programmed samples were not available) and need to program them now with our FlexGUI utility.
Can you please supply me with the config files for the standard configurations?
It would be nice to use them as templates and apply minor changes.
Another question arises when looking at the configuration report of the EU device. From the configuration point of view this seems to be the device which is used in the schematic of Boundary Devices for the Nitrogen board.
But in this schematic SW3 and SW4 are connected together for VDD_ARM. The report says that the EU starts up with 0.9V for SW3 and 0.85V for SW4, which doesn't seem to fit.
So do you know if one of the configurations EU/F1/F2 fits to the Boundary Devices board?
Regards,
Bernhard.
Hi
I check the website of Boundary, the schematic is updated and may customer should refer to the one below:
https://boundarydevices.com/product/nitrogen8m-mini/
and it should use the EU standard version.
BRs
jinyu
Hi wenhuachen, the customer had an older version of the schematic (attached).
In fact there was another question in my initial request:
Can you please supply me with the config files for the standard configurations?
Then the customer can use the config file for the EU and make the required minor modifications and program the A0 samples he has.
Thanks,
Bernhard.
Can you please share schematic of Boundary Devices board you are referring to? BD has many version, EU should match the latest version but I don't know which one BD is published.
Hi Jinyu,
It should be E8, I will talk with team whether E8 can be set as a standard PN. Thanks.jinyuzhang