AnsweredAssumed Answered

QN9080 not advertising when advertising interval is set  to 20 to 30 seconds

Question asked by Bhavesh Shah on Aug 5, 2019
Latest reply on Aug 6, 2019 by Estephania Martinez

Hello there

 

I am using  MCUXpresso IDE v10.3.1 [Build 2233] [2019-02-20] and SDK v2.2.0.

I am testing the qn908xcdk_wireless_examples_bluetooth_power_profiling_freertos example code.

After pressing the button 1 four times controller goes into the deep sleep mode 3 sand start advertising. By default the example is having the adverting interval between 1 to 2.5 sec. 

I am able to change that interval by using the macro = time interval (in ms) / 0.625 ms, where the macro is assigned into gReducedPowerMinAdvInterval_c and gReducedPowerMaxAdvInterval_c intervals. 

I am able to successfully set the interval of 10 to 20 seconds. by setting the macros to 16000 and 32000, and it works.

But when I need to set advertising interval to 20 to 30 seconds, I do not see any adverting form the controller on mobile app.

 

Can anyone help me to resolve this issue

 

Regards,

Bhavesh Shah

Outcomes