AnsweredAssumed Answered

LPC802 Vref使用LDO供电,在VDD之后使能,VDD有瞬间拉低

Question asked by will zhang on Aug 4, 2019
Latest reply on Aug 15, 2019 by ZhangJennie

使用LPC802进行设计,需要使用ADC资源;设计上使用DCDC对VDD进行供电,使用一个LDO为Vrefp提供电压,Vrefp管脚的滤波电容1uF+0.1uF;LDO上电顺序在VDD之后,上电瞬间VDD有被拉低的脉冲;

 

问题:1)Vrefp可以在VDD之后上电么?还是必须两者一起上电?

           2)查阅DS(1.6版本的),44页 Table 13. Power consumption for individual analog and digital blocks,ADC部分 61-78uA,理论上不会导致Vref 的LCD使能时VDD的DCDC瞬间拉低;是否可以初步判定问题的原因“不是LPC802 Vref供电在VDD之后”引起的?

Outcomes