We use imx6dl sabresd board and build Android8.0
We just build with nxp BSP source code(no more modify the code) and run on sabresd demo board.
When Ethernet port connect to Gita switch appear "fec 2188000.ethernet eth0: Link is Up - 1Gbps/Full - flow control off" (network can not work)
When Ethernet port connect to10/100 switch appear "fec 2188000.ethernet eth0: Link is Up - 100Mbps/Full - flow control rx/tx" (network can work).
please help.
thank you.