If the NVCC_xxx supply can be combined with VDD_HIGH_IN and VDD_SNVS_IN in IMX6ULL designs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

If the NVCC_xxx supply can be combined with VDD_HIGH_IN and VDD_SNVS_IN in IMX6ULL designs

1,132 Views
vadimaleynikov
Contributor III

Does the NVCC_xxx supply can be combined with VDD_HIGH_IN and VDD_SNVS_IN in IMX6ULL design?

Labels (1)
0 Kudos
5 Replies

932 Views
igorpadykov
NXP Employee
NXP Employee

Hi Vadim

this is not allowed as datasheet sect.4.2.1 Power-Up Sequence requires 

VDD_SNVS_IN supply to be turned on before any other power supply.

i.MX 6ULL Applications Processors for Consumer Products

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

932 Views
Rodrigue
NXP Employee
NXP Employee

HI Igor,

Is there any reason why it differs from the i.MX6UL where both supplies can be tight together?

br,

Rod

0 Kudos

932 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rod

 

>Is there any reason why it differs from the i.MX6UL where both supplies can be tight together?

I thnk it has similar design as i.MX6UL and the same power-up sequence.

Best regards
igor
0 Kudos

932 Views
Rodrigue
NXP Employee
NXP Employee

Then which one is right? 6UL or 6ULL?

And then we have to correct the Datasheet

Br,

Rod

0 Kudos

932 Views
igorpadykov
NXP Employee
NXP Employee

Hi Rod

I think both are right.

pastedImage_1.jpg

Best regards
igor

0 Kudos