AnsweredAssumed Answered

AD detection is not allowed

Question asked by yang wei on Aug 1, 2019
Latest reply on Aug 5, 2019 by Daniel Martynek

The accuracy of the ADC is not accurate. I used the ADC0 channel 13 (PTC15) to detect the voltage. But I found that the 3.3V is the ADC value is 1023, (ten-bit resolution), but I detected 2.5V is the ADC value of 808, already The 0.1V is worse. What's even more strange is that the ADC value I detected for 0.5V is 78. This variation is already very large. Can help me check if my location problem or other problem, I will attach my code configuration

Outcomes