hi,
i find function< ZPS_vSetOverrideLocalMacAddress function > at JN-UG-3048, but cannot find it in sdk JN-SW-4170.
i want modify macAddress to simulate a lot nodes by one JN5169. i will change the mac address and try to join the network to test the max nodes my network support. i am using JN-AN-1229 to do the work.
so,
1. how can i use the fun ZPS_vSetOverrideLocalMacAddress, which sdk i should use.
2. how can i simulate a lot nodes by one 5169
thanks a lot.
Hi Xu,
This address is stored locally in the index sector of Flash memory
The mac address is configured before the ZPS_eAplAfInit. However, the API is using by the OTA Cluster.
Caution: If required, this function must be called before the ZigBee PRO stack is initialized.
Regards,
Mario