AnsweredAssumed Answered

Debugger probe J-Link from Segger not printing messages to J-Link RTT Viewer

Question asked by Jose Carlos Cazarin Filho on Jul 31, 2019
Latest reply on Aug 6, 2019 by Jose Carlos Cazarin Filho

I`m not sure if this is a problem with anything related to the NXP software

 

But I was working with some legacy projects and I was able to get output from the debugger using the follownig command

 

SEGGER_RTT_printf(0, " INIT MAIN LOOP\r\n");

 

But I updated the MCU Expresso version from 10.3 to 11.0.0 build 2516 and it is not working anymore

The program executes the above line but I can`t see any output in the Segger J-Link software, and the only thing that changed was the IDE vesion

 

Can anyone help me find out what may be the cause of this problem?

 

Kind regards

Outcomes