AnsweredAssumed Answered

Read/write S32K144 firmware version number via SWD interface?

Question asked by Perig Vennetier on Jul 30, 2019
Latest reply on Jul 31, 2019 by Perig Vennetier

Hello,

 

I have a SOC system that has SWD interface to my S32K144. I am not the one coding but I have more of a general questions as I am told that it is not doable but I have my doubts.

 

We have firmware programming function for the chip from SOC to the S32K144.

 

I'd like to be able to store a firmware version number as part of tracking of the programming sequence. Something simple that will represent something like a version "5.1" or something similar.

 

Is that doable via SWD interface and if so any generic pointers on where to look for information that I could relay to the main parties involved in our project?


Thanks!

Outcomes