aung myat

Multiple CAN ID via CAN0 MPC5744P

Discussion created by aung myat on Jul 30, 2019
Latest reply on Aug 1, 2019 by Constantin Razvan Chivu

Hi,

 

How can I configure model based toolbox of MPC5744P to be able to receive multiple CAN message on a single channel(CAN0)? I am planning to toggle red LED if I receive one CAN ID and toggle green LED if I receive another CAN ID. I could only receive a single message so far. I have attached my simulink model which is the modified version of the example which came with the toolbox. 

 

Moreover, I could not select blocking mode in the send or receive block. The following message pops up whenever the blocking mode is chosen.

Thanks!

Joe

Attachments

Outcomes