AnsweredAssumed Answered

MCU-BOOT middleware missing from New Project

Question asked by ivekengineer on Jul 22, 2019
Latest reply on Jul 24, 2019 by Robin_Shen

I recently downloaded SDK 2.6.0 for an MKV58 device.  When I built the SDK, I chose the mcu-boot middleware component.  The component is in the SDK zip file.  However, when I attempt to create a New Project using MCUXpresso, MCU-BOOT is not an available middleware component to select.

 

Obviously, I can build my own generic project and use the source code to achieve what I want, but I seem to remember this being a managed component option in the past?  is this a bug, or is the middleware component only available as source code that I have to manually import?

Outcomes