AnsweredAssumed Answered

imx6 camera input resolution?

Question asked by k ms on Jul 21, 2019
Latest reply on Aug 5, 2019 by k ms

I am using the camera in IMX6Q.

The camera resolution setting is used as follows.

1. 1920x1080@30

2. 1440x1080@30

3. 752x582@30

 

Resolution 1 and 2 work well from camera input to output. But 3 is output as if there is no input from the gstreamer.

 

Is there a range of resolutions for which IMX6Q can be input?

I thought I only needed to set act_sens_conf and sens_frm_size.

 

 

regards!

Outcomes