Hello,
I am using LPCXpresso to program the NHS3152 chip. I've had success opening the IDE and flashing programs to the chip. However, the IDE often does not open during start up and the vast majority of the time, it will stop responding all together. It became slow after I activated the Free Version with an activation key. I was also able to get it to open up by creating two instances of LPCXpresso and then creating a new workspace when prompted.
I am using Windows 7.
What could be happening here?
FYI. I am getting stuck on this loading screen.
Hello Eric,
At the moment I have been trying to reproduce the same behavior you are experiencing using Windows 7 and so far I've not had a problem with the start up or loading of LPCXpresso.
Can you try to download the IDE with this link.
If the problem persists, do you mind providing your .log text document, this is located in your workspace\.metadata.
Best Regards,
Sabina