I want to use ubuntu+openocd-0.10.0+JLink to programme on i.MX 8QuadXPlus MEK CPU Board,
I need to use the command 'openocd -f ./openocd/scripts/interface/jlink.cfg -f ./openocd/scripts/target/imx8.cfg' to connect JLink and the board, how can i obtain the file 'imx8.cfg'?
there are only imx21.cfg imx25.cfg imx27.cfg imx28.cfg imx31.cfg imx35.cfg imx51.cfg imx53.cfg imx6.cfg imx.cfg in the ./openocd/scripts/target directory.
one can download the cfg file from the link in the topic as below:
https://community.nxp.com/message/1070524?commentID=1070524#comment-1070524