AnsweredAssumed Answered

NTB0104 unused pins

Question asked by Richard Webb on Jul 18, 2019
Latest reply on Jul 25, 2019 by Richard Webb

We are using the NTB0104GU12 device to interface 1.8V logic (VCCA=1.8V) to 3.3V logic (VCCB=3.3V).

On a number of devices, we haven't used all the IOs, so have connected the A side IO to GND but left the B side IO floating.

Will this cause any problems during operation, as I noticed in the notes field in the Datasheet on page 6 that it says:

"[1] The A and B sides of an unused I/O pair must be held in the same state, both at VCCI or both at GND."

 

Thanks in advance.

Richard.

Outcomes