CodeWarrior License Server migration to Windows 10: Floating license doesn't work

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior License Server migration to Windows 10: Floating license doesn't work

871 Views
sanjay_gangadha
Contributor I

After Migrating to windows 10 floating license is not working in client machines.

I was using code warrior floating license in windows 7. After migrating to windows 10 license is not working in client machines. I have followed all the steps as per the floating license installation guide lines and all the necessary settings has done in LMTOOLS.

2019-07-17_10h29_05.png2019-07-17_10h30_00.png2019-07-17_10h30_26.png

In the host server license is working fine. But client Machines License is not accessible.

2019-07-17_10h57_20.png

Labels (1)
0 Kudos
1 Reply

746 Views
TomasPaez
NXP Employee
NXP Employee

Make sure the license file is being seen by CW app, MCU subfolder is the default location.

I also suggest to create a new service on the server Side, on Config Service Tab you can type the name of a new server and set up the service again.

Check the following community on also checking that lmgrd is running

Software Licensing 

0 Kudos