AnsweredAssumed Answered

REGISTER ACCESS IN MCUXPRESSO

Question asked by Apurv Marathe on Jul 17, 2019
Latest reply on Jul 17, 2019 by Jing Pan

Hello,

While programming the FRDM-KV31F board with the MKV31f512vll12 controller using MCUXPRESSO

I need to check if the OSCINIT0 bit in the MCG_S (i.e. Multiplex Clock Generation Status) reg is set. Now I am trying to use the and bitwise operator for the same is there any way I can directly access this bit? I know I can access the Status register via a dot operator as it is a member of the MCG structure, but still is there any way I can directly access the specified bit?

Regards,

Apurv.

Attachments

Outcomes