AnsweredAssumed Answered

VisionSDK_S32V2_RTM_1_3_0 problems

Question asked by Yung Lin Chang on Jul 16, 2019
Latest reply on Jul 25, 2019 by bpe

While reading VisionSDK_S32V2_RTM_1_3_0 userguide. Some questions occurred at 3.3.1 and 3.3.2. 

 

3.3.1 General Preparation
Export necessary environment variables:
o export ARCH=arm
▪ Target architecture
o export CROSS_COMPILE=aarch64-linux-gnu-
▪ Compiler prefix specification
o export LINUX_S32V234_DIR=/linux/sources/directory/for/s32v234/    //THIS ONEEEEEEEEEEE  
▪ optional, only for s32v234 Linux build
▪ Path to the Linux sources (same kernel as is running on the board)
o export PATH=/path/to/your/compiler/binaries:$PATH  //THIS ONEEEEEEE
▪ Path to the compiler binaries

 

Can some one give me an real example?

 

3.3.2 Building the Kernel Modules
Following kernel modules can be built:
• apex.ko:
s32v234_sdk/libs/apex/drivers/kernel/build-v234ce-gnu-linux-d

 

I got this           '' Please define LINUX_S32V234_DIR pointing to kernel directory . ''

 

If it the same thing as 3.3.1 , a real example plz.

 

 

Outcomes