AnsweredAssumed Answered

Errors to build core-image-minimal-initramfs

Question asked by jupiter hce on Jul 13, 2019
Latest reply on Jul 19, 2019 by Aldo Gutierrez

Hi,

I tried to build zImage-initramfs, I could not run following command, what I could be missing?

 

$ MACHINE="solar" DISTRO="solar" bitbake core-image-minimal-initramfs
ERROR: Nothing RPROVIDES 'initramfs-module-install'
initramfs-module-install was skipped: incompatible with host
arm-oe-linux-gnueabi (not in COMPATIBLE_HOST)

 

Also, that meta-freescale/wic/imx-uboot-bootpart.wks and other wks files are all used for creating SD card image, how can I change the image configuration for wic or zImage-initramfs running on RAM? Which command to add u-boot argument such as bootargs, bootcmd, console, etc., to run u-boot and zImage-initramfs by imx6 uuu on imx6 RAM?

 

Thank you .

Kind regards,

- JH

 

 

Outcomes