Two uart issues at least from official bsp 4.1.15 to 4.19.35

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Two uart issues at least from official bsp 4.1.15 to 4.19.35

763 Views
csoapy
Contributor III

1.  Not aware of CONFIG_MAGIC_SYSRQ

drivers/tty/serial/imx.c: In function ‘serial_imx_save_context’:
drivers/tty/serial/imx.c:2355:47: error: ‘struct uart_port’ has no member named ‘sysrq’

if (uart_console(&sport->port) && sport->port.sysrq)

    And a warning from Geetoo, https://wiki.gentoo.org/wiki/Magic_SysRQ

 Warning
Magic SysRq should not be enabled in kernel for production or mission critical systems! Even if Magic SysRq is disabled at boot using for example sysctl, it still leaves /proc/sysrq-trigger open. Not to mention the fact that re-enabling SysRq is as easy as disabling it.

2. console_unlock() takes too long time while registering console in kernal/printk/printk.c

[ 0.392208] 2020000.serial: ttymxc0 at MMIO 0x2020000 (irq = 26, base_baud = 5000000) is a IMX
[ 0.392956] 21e8000.serial: ttymxc1 at MMIO 0x21e8000 (irq = 68, base_baud = 5000000) is a IMX
[ 1.200683] console [ttymxc1] enabled
[ 1.204851] 21ec000.serial: ttymxc2 at MMIO 0x21ec000 (irq = 69, base_baud = 5000000) is a IMX

   A similar issue but fixed in 2013: [3/3] printk: Avoid softlockups in console_unlock() - Patchwork 

   And at least 3 people have the same problem from 2016 to now

         4.1.15 BSP register_console  issue

         https://community.nxp.com/thread/468205

         android6.0 imx6q & imx6dl kernel boot very slow (two issue)

         https://community.nxp.com/thread/447906

         1s time pause on console when kernel boot

         https://community.nxp.com/thread/440825

Labels (2)
Tags (4)
0 Kudos
1 Reply

513 Views
b36401
NXP Employee
NXP Employee

Here is some information regarding to sysrq:
https://community.nxp.com/message/336619

0 Kudos