AnsweredAssumed Answered

LPC55S6x CPU1CLKEN bit questions

Question asked by Isao Takashima on Jul 10, 2019
Latest reply on Jul 10, 2019 by Alice_Yang

I create sample project for CPU0 and CPU1 of LPC55S69 using LPC55S69-EVK and EWARM ver 8.40.1.

I can debug the project for CPU0, but I cannot debug the project for CPU1.

If I set CPU1CLKEN in the CPUCTRL register to 1, I can debug the project for CPU1.

Therefore I believe that the following description of CPU1CLKEN in the user manual rev 1.3 is incorrect.

   3   CPU1CLKEN   RW        CPU1 clock enable. 0x1
                                          0  The CPU1 clock is enabled.
                                          1  The CPU1 clock is not enabled.

I believe that we need to set CPU1CLKEN to 1 to enable CPU1 clock.

Am I correct?

 

Please reply as soon as possible.

 

Best regards,

Takashima

 

Outcomes