RT106x external interrupt sources

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RT106x external interrupt sources

1,050 Views
mszczygi
Contributor I

Hi,

Is there a document that describe assignment of external interrupt sources to interrupt controller in i.MX RT1060/1064?

What I'm asking is, for example, I have a external trigger source, like push button, connected to GPIO pin that should trigger interrupt handler function. I'm designing hardware base on i.MX RT1060 and I'd like to know which GPIO's pins can be used as source for external interrupt. In my experience with ARM Cortex-M micro-controllers only certain number of GPIOs can be assign to function as trigger sources for external interrupts.

Best regards

Mariusz

0 Kudos
1 Reply

945 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Mariusz,

Regarding your following question: "I'd like to know which GPIO's pins can be used as a source for external interrupt". You can find this information on Table 3-2 of the reference manual.

pastedImage_1.png

Also, within the SDK for the RT1060-EVK you will find an example named igpio_input_interrupt. This project triggers an interrupt each time you press a button from the evaluation kit. You can use this project as a base to create your own. 


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos