AnsweredAssumed Answered

STM comparator and timer equivalence pin

Question asked by Javier Hernandez on Jul 4, 2019
Latest reply on Jul 4, 2019 by Mark Butcher

Hello,

 

I need use this stm pins of the comparator in kl05.

 

PA0.Signal=COMP1_INM6
PA1.Signal=COMP1_INP
PA4.Signal=COMP1_INM4
PA5.Signal=COMP1_INM5

 

Wich is the equivalence in MKL05Z32VFK4? In the datasheet only is possible to found CMP0_INx and CMP0_OUT. It's ok if I use only the inputs? CMP0_IN0 up to CMP0_IN3 ?

 

 

And I have the same problem with the Timers: I have used from TPM0_CH0 up to TPM0_CH5. It will work?

STM32                                         KL05

PA7PA7.Signal=TIM1_CH1NPTA5TPM0_CH5
PA8PA8.Signal=S_TIM1_CH1PTB9TPM0_CH2
PA9PA9.Signal=S_TIM1_CH2PTB10TPM0_CH1
PA10PA10.Signal=S_TIM1_CH3PTB11TPM0_CH0
PB0PB0.Signal=TIM1_CH2NPTA6TPM0_CH4
PB1PB1.Signal=TIM1_CH3NPTB8TPM0_CH3

 

Best regards

 

 

EDITED: I think that COMPx_INMx is the negative and the COMPx_INP the positive but in NXP is indifferent?

Outcomes